Reliable latch technology in a lightweight package

Friday, November 18, 2011 by Daniel McCourt
Electronic rotary action latch light dutyIt seems like everyone is dieting these days…even our products. The new R4-EM Light Duty Electronic Rotary Latch brings the same proven reliability of the standard steel version but has lost a bit of weight—65% to be exact, thanks to its engineered composite plastic construction. But don’t be misled by the compact package; this latch is big in performance.

A microprocessor control brings energy efficiency, and an integrated mechanical override is included for use should a power failure occur.

Need to know the latch status? The optional microswitch will let you know when the door is locked or unlocked. And if you want to monitor and control complete systems remotely, it’s all possible with this latch. Southco Indutry Solutions

The R4-EM is simple to use, simple to install and is concealed for hidden access. Add a 12-24 volt DC power supply (and any access control device), and you have a complete electronic access solution.

Visit our website for more information on the entire line of Rotary Latches or any of our other latches, hinges or electronic access solutions.
 
What do you think of the new R4-EM? Drop us a line.

Innovative Southco Marine Hardware Solutions

Tuesday, November 1, 2011 by Daniel McCourt

METS Logo
The Southco Marine team is happy to invite you to our booth at this year’s METS exhibition between 15-17th of November.

Come and see our Innovative Marine Hardware Products and our extended product offering, and explore how our team can help you with solutions for entry, cabin, and deck applications.

The show will be hosted at the Amsterdam RAI Convention Centre in The Netherlands. For registration details and accommodations visit www.metstrade.com.

We look forward to seeing you!

Welcome!

You will find us at Hall: 3 Booth: 414

Two new actuators, one great list of benefits

Friday, October 21, 2011 by Daniel McCourt
On siteIf you’ve ever taken a good look at off-highway equipment that has been left outdoors and exposed to the elements, then you know the damage that is visible from rain, heat and cold.  Well, Southco’s new line of actuators are here, and they are as tough as the elements and are designed for entry door applications. The AC-30 and AC-40 are constructed of corrosion resistant materials and can be used in a wide range of outdoor temperatures.

Both actuators work with Southco R4 rotary latches directlSouthco Actuatory or can be used with cables and rods for a complete rotary latch system. Your equipment will be secure on the job site or roadside due to the key-locking feature with multiple key codes.

The AC-30’s single hole installation enables effective mounting in restricted spaces, and the AC-40 features a large grip handle and single-motion open feature. With the addition of these new actuators, Southco has an even great line of solutions for your most challenging applications. Tell us about it. Or leave a comment. We love to hear from you.

Ten questions to ask when designing in a hinge

Thursday, October 13, 2011 by Daniel McCourt
Part 10 in a 10-part series on specifying hinges

checklistWe spent the last several weeks discussing different factors for specifying hinges. After all, incorporating hinges early into designs helps keep costs down and options open. So here, for your reference, is a quick summary of questions to ask in the early stages of your application. They will save you time, money and maybe even a bit of frustration!
  1. How much load must the hinge withstand? Determine the size, weight, and center of gravity of the door.
  2. How do hinges fit in the overall design? Designing the hinge in early may allow use of an available hinge.
  3. How much space can you afford inside or outside the enclosure? This may help you decide between concealed and externally mounted hinges.
  4. How do you plan to mount or access the door? Door and frame configurations play a critical role!
  5. How far must the door open? Detent and friction hinges will keep a door open without secondary mechanical supports.
  6. Is removing the door a requirement? Lift-off hinges enable fast door removal.
  7. What specifications must the hinge and enclosure meet? Many hinges are certified to meet various industry standard specifications.
  8. How will the hinge be installed? Consider the manufacturing and installation process carefully.
  9. Do you need to meet specific material requirements? Think about environmental conditions the end product may face.
  10.  How large a role do aesthetics play in the design? Balance performance needs with style and appearance.
To learn more about any of these topics, please see the past weeks’ blog entries, which discuss each of these questions in greater detail. Or contact us personally. We'd love your feedback and questions.

Hinges and aesthetics

Thursday, September 29, 2011 by Daniel McCourt
Part 9 in a 10-part series on specifying hinges

Design guyOkay, so you’re looking to optimize the overall quality and cost effectiveness of your application. When it comes to hinges, it is important to balance performance needs with aesthetic judgment. Looks DO matter and can greatly influence a product’s overall look and perception of quality.

Large, external hinges give an impression of great strength whileDetent hingeFriction hinge concealed hinges can increase security or create a streamlined look. To further enhance an application’s design, we often have the option of customizing plastic and powder-coated hinges to suit specific color specifications. Some hinges even include snap-on covers to conceal mounting hardware and create and more polished appearance. Even the mounting hardware can be concealed by installing the hinge from the back side of the door.

Stainless Steel HingePolished hingeWhether you want polished and sleek or sturdy and strong, there is a hinge that will convey the appearance you seek and contribute to the overall aesthetic of your application.




Next week: Ten questions to ask when designing a hinge

Hinges and Material Requirements

Wednesday, September 21, 2011 by Daniel McCourt
Part 8 in a 10-part series on specifying hinges

Sheet_metalThere are many factors to consider when selecting a hinge. We have discussed opening angle, frame configuration, industry specs and installation method, among others. But a critical consideration not to be overlooked may seem like the simplest: material.

When deciding between material options, be sure to consider not only the end uszinc torque hingee but alsostainless steel hinge environmental conditions. Factors from temperature range and chemical exposure to UV radiation and moisture conditions can (and should) influence our choices. As you well know, hinges comes in a variety of materials such as steel, stainless steel, die-cast zinc and engineering plastics. Each of these materials brings with it certain great benefits.
Plastic Hingestainless steel lift off hinge
Steel and stainless steel hinges withstand temperature variations, and engineering plastics and stainless steel offer corrosion resistance. Need reduced noise and vibration? Consider a plastic hinge. Whatever your need or application, there is a hinge material perfectly suited to it. Need help finding one? Contact Southco or share your thoughts on this discussion.

Next week: Hinges and aesthetics

Hinges and Installation Method

Friday, September 16, 2011 by Daniel McCourt

 Part 7 in a 10-part series on specifying hinges

InstallationThe method of installation is an often overlooked consideration when selecting a hinge. Manufacturing tolerances in the design and installation process can impact our hinge specifications, especially where aligning the hinges on the door and frame are concerned. Slotted holes may help compensate for manufacturing variations.

An important questions that we have to ask is: Where in the manufacturing process is the hinge installed? This may have a profound impact on hinge selection. It’s helpful to determine whether the leaves will be assembled to the door and frame at the same time or in different locations and assembled later. Mounting methods run the gamut and include screws, studs, rivets, welds and adhesives.

Lastly, you want to determine clearance for any tools needed for installation (as well as the hardware itself).  Most of us have found ourselves in this unfortunate situation at least once! So don’t get stuck at the end. Figure this out early and save yourself time and aggravation.

Next week: Hinges and material requirements


Hinges and industry specifications

Monday, August 29, 2011 by Daniel McCourt

Part 6 in a 10-part series on specifying hinges

standardsSelecting the proper hinge can sometimes be more challenging that we might expect. In addition to considering cost, aesthetics, strength requirements and door configurations, we need to also consider any regulations or specifications that might affect our applications. 

For example, hinges used on outdoor enclosures housing electronic equipment may be required to meet NEMA and IP standards. Is your application in the food equipment industry? NSF certification imposes stringent guidelines on materials and design.
southco hinges
Specs may require evaluation of an entire system, or hinges may be certified to meet a spec as-is. Either way, you want to select a hinge capable of meeting all product standards.

A keen understanding of industry requirements will help you select the best hinge for your application (and will save you time and money in the process!).

Next week: Hinges and installation method

Removable hinges and interior access

Thursday, August 18, 2011 by Daniel McCourt


Part 5 in a 10-part series on specifying hinges

ServicemanSometimes a user or service technician requires full access to the interior of a cabinet or enclosure. If this is the case,  lift-off hinges or hinges with retractable pins can make it quick and easy to remove a door. You’ll also find these hinges valuable if a product ships unassembled or if the door and frame are manufactured in different locations.

Lift-off hinges let you remove the door in a single motion (withoutLift Off Hinge using tools). Just lift the door off the hinge pins mounted to the frame, and replace it by lowering it back over the hinge pins. Both your hands will remain free to maneuver the door. It might be a two-person job at most, but you’ll be amazed at the ease and speed of removal these hinges allow.
 
Hinges with retractable pins enable door removal without ever having to lift it. You retract the hinge pins and pull the door straight off. To replace it, you would just need to align the two halves of the hinge, Pin Lift Off Hingeextend the pins and lock the door back into place. Quick and very simple. While hinges with pins permanently attached won’t let the hinges drop or get lost, retractable hinge pings might be a better choice if the hinge axis is not guaranteed to remain vertical and steady.

Next week: Working within industry specifications

Considering the opening angle: Detent and torque hinges

Monday, August 15, 2011 by Daniel McCourt

Part 4 in a 10-part series on specifying hinges

Door StayWe have all been there: Trying to keep a door open with our foot, a shoe or something else we find lying around. Today’s applications increasingly require hands–free access (or a really patient friend who will hold the door for you). If this is the case with your application, consider using a hinge with a built-in detent feature to hold the door  or panel open at a preset angle. Or use an adjustable-torque feature, which will let you tighten or free up the door swing. Both of these hinge styles eliminate mechanical supports like gas struts or door stays.

Detent and torque hinges are two products in one—the hinge and the doorDetent Hinge stay. They bring with them some nice benefits, too. They reduce the number of parts, cut down on installation time and lower the overall cost.

Most detent hinges come with preset opening angles; some even provide negative angles that let the hinge go slightly past center when closed. This also holds the door securely against the frame and Torque Hingereduces vibration (a viable option when you know you might have rattling!). In some cases, you won’t even need a latch. Detent hinges are most appropriate for small lightweight applications. If this sounds like your application and you can benefit from some of these features, give it a try!
 

Next week: Using removable hinges to access an interior

Deciding between concealed and externally mounted hinges

Friday, July 29, 2011 by Daniel McCourt
Part 3 in a 10-part series on specifying hinges

Access PanelWe’ve discussed how important a consideration strength is when selecting a hinge. Now it’s time to examine the design considerations that sometimes dictate whether we select a concealed or externally mounted hinge.

Concealed hinges mount on the interior part of the door and frame. They are great to use when you desire a clean outer panel (and you get the added benefit of vandal resistance). When using an internal hinge, just remember to consider the amount of internal protrusion since inside space may be limited. These hinges may also restrict access and make it hard to install and hide mounting hardware. Since they work with specific doors and frames, product and mounting options should be designed with them in mind. Used appropriately, internal hinges deliver a sleek, streamlined appearance.Stainless Steel Lift Off HInge

Exposed, external hinges deliver a different set of benefits: they work with limited interior space, offer greater strength and allow for a greater door-opening angle. Unlike concealed hinges, they are easy to fit to an application anytime in the design process…and they are more universal. They of course won’t be hidden, so care should be taken to blend the hinge design with the application.

Next week: Door and frame configuration and flexibility with opening angles

How strong of a hinge do you really need?

Tuesday, July 19, 2011 by Daniel McCourt
Part 2 in a 10-part series on specifying hinges

Stong ManLast week we discussed how strength is often one of the first considerations when choosing a hinge. But just how strong a hinge do you need?

Here at Southco we use four factors that can help when getting started.

1. Weight: Determine the weight of the door. If you can’t physically weigh the door on a scale, a quick estimate can be calculated with the following formula: length x width x height x density. The heavier the door, the stronger the hinge you will need.

2. Center of Gravity: Determine the center of gravity (Cg) of the door. If the door is uniformly thick, the Cg will lie dead center. Unfortunately, most doors aren’t uniform.

So here’s a few simple steps for determining the Cg, regardless of door shape.

(A) Hang the door from one corner so it pivots freely Hinges
(B) Attach a plumb line to the pivot so the line hangs freely
(C) Mark the line on the door
(D) Repeat twice more, hanging the door from a different corner each time

The Cg is where all three lines intersect.

3. External Loads: Consider the added weight of components that might be fastened to the door: electronics, cooling equipment, hooks, etc. And don’t forget loads applied by wind, moving objects or forces generated by gasket compression or pressure within an enclosure.

4. Test:  Whenever possible, test the hinge in the application. Variations in mounting and build tolerances often mean that one hinge takes the brunt of the load. We need each hinge to share equally in the effort!

Next week: Considering overall design and deciding between concealed and externally mounted hinges.


Design News Article on Designing for Recyclability

Wednesday, July 13, 2011 by Daniel McCourt
Design News LogoDoug Smock over at Design News wrote a great article on Designing for Reyclability this month.  He highlighted the trend towards designing for dissasembly and the key role that fasteners, hinges and latches can play in this effort.

We here at Southco couldn't agree more! Head on over and check it out.

Incorporate hinges early to save money and frustration

Tuesday, July 12, 2011 by Daniel McCourt
Part 1 in a 10-part series on specifying hinges

External HingesIt is not uncommon to wait until the last minute to incorporate hinges into a design.  We know that not everyone has hinges at the top of their list of important things to think of when working on a new car, enclosure, or life-saving medical device.. However, considering hinges late in the design cycle can limit your options. You might have to compromise your design or force nonstandard parts into your product risking increased cost and reduced performance.

Over the next 10 weeks, we will examine multiple factors to consider when specifying hinges. Keep these tips in mind, and you’ll keep your options open (and your project costs down).


Let’s start with one of the first considerations when it comes to hinges: strength.

StrengthHow much load will the hinges bear?  And many times it’s not just the weight of a door but all external sources of load. Will equipment be mounted on the door? Make sure to account for dynamic loading.

Another tip to keep in mind: the as the ratio of door width to height increases, so too do the stresses. For maximum strength, place hinges as far apart as possible on the longest edge of the door. Or, depending on the design, use a closer hinge spacing to stiffen the door or ensure sealing against a gasket.


Next week: How strong a hinge is needed? I’ll share four specific factors (and a handy formula) to help you out.

A simple push toward greater convenience

Tuesday, May 24, 2011 by Daniel McCourt
If you’ve ever accidentally closed a door or panel with a traditional cam latch in the closed position, then you know the damage that can occur over time to the door, frame or latch. I have been guilty of this many times myself…

Push to close latchNow, Southco has expanded its E5 Cam Latch selection by adding intuitive push-to close convenience to more than a dozen hand-, tool- and key-actuated models. The push-to-close design prevents damage to the latch regardless of the cam position during closing. A spring-loaded feature automatically engages the cam once it passes the edge of the keeper or frame.

What’s even better is that the new designs satisfy both single-pointE5 Bus and two-point latching options. We all like convenience, and our cam latch installations should be no different! A latched/unlatched status indicator provides users with quick visual confirmation of latch status, too, so there is no more guesswork about whether your panel or door is secured.

E5 EquipmentWhether your application is office furniture, an RV or an electronic enclosure, the E5 has a design and configuration to fit your needs. Simplicity, versatility and flexibility.

To discuss how the flexibility of the new cam latch can enhance your application, send us an email or post a comment.

IFSEC 2011

Monday, May 16, 2011 by Daniel McCourt
Join Southco at the IFSEC 2011 Tradeshow this week.  We will be displaying our latest Electronic Access Solutions at the Isonas booth, Hall 4 4/E160d.

IFSEC 2011Our Applications Engineers will be on hand to answer your toughest implementation challenges.

We look forward to seeing you there!

If you are unable to attend, feel free to email our customer service, available around the world 24/7. They are available to discuss electronic access solutions or any of Southco's 40,000 latches, hinges, or locks.

About IFSEC:

IFSEC is the largest annual security event in the UK.

This year's show saw IFSEC continue to offer unrivalled security solutions to more than 22,743 security professionals.

Dedicated to offering all things security, IFSEC offers you the full spectrum of security products and services available both in the UK and worldwide. Housing 600+ leading manufacturers, suppliers and distributors, the 2010 event had a global reach of over 22,743 attendees from 130 countries and was supported by all industry associations and countless media.


Southco's New Membrane Keypad

Wednesday, May 11, 2011 by Daniel McCourt
Membrane KeypadIt's always nice when a respected publication like PD&D puts one of our new products on their website.

The latest new product to be placed on their site is our EA-KC2 Membrane Keypad Access Controller.

This new keypad can adhere to a frame or door, inside or out. The ability to adhere or be molded into a wide variety of surfaces, combined with connecting it to any one of our Electronic Latches or Locks  brings electronic access to applications that would not have been possible just a few years ago.

Please leave a comment or email us if you would like to hear about some examples of how this new technology is being used in the marketplace.

The EML Goes High(er) Tech

Thursday, April 7, 2011 by Daniel McCourt
There is no question-- electronic record keeping is now the norm. But as the technology has advanced, so too has the opportunity to exploit it. Fortunately, a unique partnership has Biometric Electronic Latchresulted in the industry’s first biometric-integrated latch for computer server racks. Southco has teamed with Digitus Biometrics to secure data right down to the rack level in datacenters.

The db ServerRack access control system marries Southco’s proven H3-EM Electronic Locking Swinghandle with a built-in, multi-stage fingerprint verification and access control system from Digitus Biometrics. It sounds very “CSI,” but it’s actually quite simple and very effective.

The access control unit connects directly to a datacenter’s network via an fingerprintordinary connector. User access to cabinets is then managed from a single desktop. No more keys, cards or PIN pads. And 100% accurate validation! Interfaced with a monitoring network, the system can remotely account for all rack activity, including who accessed it, when it was accessed and the duration. An audit trail has never been simpler. The new db ServerRack access control system includes all needed software and is easily and conveniently retrofitted into existing enclosures. 

To view Southco's entire line of Electronic Latches visit our new dedicated Electronic Access Solutions Mini-site and download a copy of our electronic latching guide.

Stainless Steel Rotary Latch Designed to Meet Challenges of Marine Industry

Tuesday, March 1, 2011 by Daniel McCourt
The ocean can be as unforgiving as it is beautiful when it comes to the harsh effects the sea can have on hinges, latches and other boat hardware.
Stainless Steel Rotary Action Latch
Southco understands the need for a reliable rotary latch that can withstand salt, sun and the damaging effects of water. Hence, the Stainless Steel R4-10 was introduced. The new R4-10 features the same benefits of its zinc-plated predecessor with a finish that delivers durability and corrosion resistance. Constructed of 304 grade stainless steel, the latch can be used in demanding vandal-proof or watertight storage areas with the assurance that its construction meets marine requirements for performance and salt spray resistance. So no more rusted hardware!
 
The R4-10 even offers double stage latching for added security and functionality, so you can rest easy knowing that your belongings are secured against vandals. And a concealed latching option allows flexible styling while the latch accommodates misalignment for a flush, consistent look. The new AC-M1 actuator makes a nice addition, too. It is constructed of 316 grade stainless steel and delivers corrosion resistance and enhanced security.

We want to hear from you! Contact us with your questions or comments on the stainless steel R4-10. Or to learn more about Southco’s line of rotary latches, email us or visit our site at http://www.southco.com

The Mini E-Keeper: A little package with some big benefits

Tuesday, February 1, 2011 by Daniel McCourt


It’s 2/3 the size of its big brother, features an integrated mechanical override and boasts a more efficient gear motor. Meet the Miniature E-Keeper System—a slimmed-down access solution that provides push-to-close operation in one unit.

Southco Miniature Electronic StrikeThis compact unit means that transitioning from mechanical solutions to electronic access solutions could not be simpler. It’s easy to install and can be added right to a frame for use with existing latches. If security is a major concern, it can mounted in a concealed location with remote mechanical override. Which means—yes—it is perfect for applications like medical storage units, postal terminals and other secured enclosures. Put simply, it is designed to simplify access while providing convenience, security and control.
vending machine
Another great thing about the Mini? It’s flexible. So it’ll work with keypads, key fobs, card swipes…an array of different actuation devices. That versatility means you can integrate the specific level of secure access control you require. It accommodates multiple mounting configurations, too, so it can be easily integrated into existing designs. Ahh…secure electronic or manual operation without having to modify enclosure designs. That’ll make OEMs happy!

To share your thoughts on the E-Keeper or learn more about Southco’s complete system offerings, leave us a comment here. We’d love to hear from you!


The Business Blogging Platform Powered by Compendium  |  Sitemap