Electronic Access Latching Helps to Deter Theft

Wednesday, April 25, 2012 by Rachel Pilgren

When it comes to locker use, winning the war against theft can be tough. Whether an employer requires its employees to keep their belongings in a locker during their shifts, or a business offers lockers for customer use, security must always be at the forefront of operations. Because even codes to the most sophisticated combination can be cracked and keys can be stolen or copied, locker manufacturers are looking at new ways to deter theft - and many are turning to electronic access solutions.

A locker manufacturer recently approached Southco engineers about specifying a latching system for an upgraded line of lockers designed to protect more valuable belongings in both work and leisure settings, such as expo facilities and athletic clubs. Its engineers were mainly interested in a heavy-duty internal latch to be housed in the locker door, as well as a more unique option for user access than a key or combination lock.

 

Our engineers recommended the EA-KC2 Membrane Keypad Access Controller and R4-EM Electronic Rotary Latch, which simplify access management with a self-contained unit, meaning no external connections or software are required to program or operate the system.

The Membrane Keypad Controller contains a microprocessor that compares the stored user access codes with what is being entered on the corresponding Membrane Keypad and either grants or denies access. The Controller also provides two outputs for independent control of two separate latches and works with the Membrane Keypad, which can hold 120, four-digit user codes.

 

The R4-EM Electronic Rotary Latch, which features a secure, concealed electronic release latching solution, can be wired into the Membrane Keypad Access Controller system and when the Controller recognizes the code entered by the user, it will release the R4-EM latch. The user need only push to close the locker door and the latch will re-secure- itself.

 

How can electronic electronic access solutions enhance your locking applications? Tell us in the comments.

Southco Sponsors Award-Winning FIRST FRC Team

Wednesday, April 11, 2012 by Rachel Pilgren

The Southco Honeoye Falls Facility is nurturing the next generation of engineers through the sponsorship of a team of local high-school students, who not only competed in this year’s regional FIRST Robotics Competition (FRC), but took the top honor against 41 teams.

FIRST (For Inspiration and Recognition of Science and Technology) was founded in 1989 to inspire young people's interest and participation in science and technology. FIRST sponsors events for K-12 students which are designed to help them discover and develop a passion for science, engineering, technology and math.

As the main focus of this year’s FRC, Honeoye’s team, the SUITS (Students Utilizing Ingenuity Technology and Science) created a robot that they used to participate in this year’s tournament, which required them to compete against other teams by executing a series of tasks for points.

The robot, which was designed and completely built within six weeks according to strict FIRST deadlines, also helped the team to secure the Rookie Highest Seed Award in addition to their victory at the Finger Lakes Regional Competition at Rochester Institute of Technology (RIT) in March.

Building a robot in only six weeks was no easy task. However, when it comes to design, Southco’s engineers are always up for a challenge. It’s only natural that Honeoye Falls’ own Rick Langkamp, Manager of Manufacturing Technology and New Product Development, would jump at the opportunity to mentor the SUITS and help them design, execute and test a robot in such a short time.

“It’s a very aggressive timeframe,” said Langkamp, who has over 28 years of experience with Southco. “It would be a stretch even if I brought it in here as a regular project.”

Langkamp is no stranger to FIRST – his own son has participated in the FIRST LEGO-League, a category for kids grades 4-8. Langkamps’s main focus as a mentor for the SUITS team is assisting them in the programming for the control system of the robot.

Langkamp, who has been with Southco since he was an engineering co-op, works primarily with mechanical and electronic controls and sensors, focusing on new product development and new manufacturing processes. He was impressed with the quality and sophistication of the software and full kit of electronic parts available to his team, which are provided by FIRST sponsors and are available to them for a full 12 months.

“We never had access to this cool stuff when I was a kid,” said Langkamp. “Imagine the potential of kids who come up through the program and what they could contribute to the future of engineering,” he said.

Southco’s products played a key role in the development of the team’s robot, said Langkamp. Scrap metal from Southco’s production facility, fasteners, latching hardware and other machined parts from the Honeoye Falls facility were used in the robot’s construction. Southco’s Information Technology (IT) team even donated several old laptops for the team to use when programming the robot.

The SUITS’ robot has a variety of advanced features and is designed to be as close to a real engineering experience as possible. Langkamp said that the robot-building process offered by FIRST is unique in that:

  • The frame is typically built from aluminum channel , similar to 80/20 aluminum.
  • A programmable logic controller from National instruments is included in the control system (These are programmed in Labview, Java, or C++).
  • A wireless network access point is incorporated, as all robots are required to run on a wireless network during the competition.
  • Electronics includes variable speed motors , switches, solenoids, servomechanisms and lighting.
  • Many robots incorporate a camera and vision system as well as ultrasonic sensors, gyros and accelerometers.
  • Teams also have the option of using a pneumatic compressor and air cylinders.
  • It is up to each FRC team to decide how they want to design their robot using Autocad, Pro- E (CREO) and other software.
  • The teams are held to a budget of $3200, with a maximum allowed robot weight of 120 lbs.

In addition to the robot design, FRC teams are challenged to raise funds, design a team “brand” and work together as a team.  With the help of their team leader, Mike Shaughnessy, the SUITS have raised over $21K to pay for their entry fees and travel costs. The SUITS also sell LED light bulbs to support their team.

“It’s just a great program,” said Langkamp. “There is something for everyone because kids involved can choose to do marketing, fundraising and finance, not just engineering.”

Look for the SUITS’ logo, a black shirt with white tie, at the FIRST Championship competition, which will be hosted at the Edward Jones Dome in St. Louis, Missouri on April 25-28. The SUITS (Team #3951) will compete against other regional winners as they contend for the top spot in the national competition.

Heavy-duty Latches Ensure Secure Storage on the Road

Wednesday, March 28, 2012 by Daniel McCourt

 

Utility VanThe utility van: mobile office for the construction industry. For contractors working out of their vans, storage plays a key role in their daily operations. If tools and materials are not securely stored, contractors could face damage to their van and tools, as well as potential  injury caused by unsecured objects. 
 
A vehicle utility contractor for a large electricity company recently approached Southco engineers regarding a latching system to secure wall-mounted storage compartments and cabinets inside its fleet of utility service vans. The company had received reports from its employees that the existing hardware was sometimes unpredictable in its operation, resulting in tools popping out of boxes while the vehicle was in motion.
 
The contractor was seeking a strong, durable latch that would stay closed when disturbed by bumps and turns while the van was in motion, as well as exposure to changing weather conditions, since the rear door of the van would be frequently opened and closed by the technician when on the job.
 
Our engineers recommended Southco’s Stainless Steel R4-10 Rotary Latch, which brings corrosion-resistant strength to a proven latching 

solution that delivers long lasting durability and security to heavy-duty 
applications. For this application, our engineers recommended combining the R4-10 with Southco’s AC-70 Single Point Paddle Actuator for a complete latching solution. When installed, the R4-10 is linked to the Actuator by a cable, which triggers the latch when the Actuator is engaged. Additionally, the AC-70’s low-protrusion, front-mount design allows for easy operation by the end user, who need only actuate the paddle with the pull of a finger.
 
With a simple push-to-close operation, the R4-10’s concealed latch accommodates misalignment between the latch and striker bolt, making it suitable for a wide variety of applications. In gasketed applications, a double stage latching option provides additional security and functionality, allowing the user to push the door once to keep it closed, and push it a second time to securely latch it, preventing a false latching condition which could result in the door opening accidentally.
 
Are you facing a challenging application that calls for a more robust latching solution or want to know more about our rotary latches or hinges? Tell us in the comments.
 

Push-to-Close Latching; The Secret of Simple Operation

Thursday, March 15, 2012 by Daniel McCourt

 

PushWhen it comes to convenience, it’s easy to take even the simplest of operations for granted. This week we take a closer look at a simple operation that often goes unnoticed: push-to-close latching.
 
Push-to-close latching technology is in everything from car doors and glove boxes to storage cabinets and office furniture. Its simple functionality allows us to securely close a panel and not have to worry about having to manually re-latch it. 
Southco e5
 
In a push-to-close application, the cam rotates freely from the "closed” 
position as it contacts the frame or keeper, and an integral spring pushes the cam back into the engaged position once the cam clears the keeper. Southco’s E5 Push-to-Close Cam Latch features push-to-close convenience by incorporating a spring-loaded ramped cam or actuator for single or multi-point operation.
 
Basically it works like this: Think about how often you open and close a cabinet door. Adding our E5 to this application means that when you push the door towards its frame, a ramp-shaped cam rotates as it contacts the frame, the cam then springs back and moves behind the frame to achieve latching.
 
E5 Push to Close OperationAs with conventional cam latches, the E5 latching mechanism rotates to disengage from the keeper, but once the panel is opened and the cam rotates back to the "closed" position, the ramp-shaped face of the retractable cam functions like a push-to-close mechanism, ensuring safe, trouble-free operation even if the door is shut with the cam in the closed position.
 
The unsung value that push-to-close operation brings to your application design is paramount. Incorporating an action as simple as not having to manually re-lock a door every time it is closed can bring great value to end users in a wide array of industries.
 
Is simplicity a priority in your application?  Tell us in the comments.
 

Slide Latching Adds Security and Style to Transom Doors

Tuesday, February 28, 2012 by Daniel McCourt

YaughtIt’s no secret that yacht design is all about the details. These large luxury vessels are built to complement the luxe tastes of their buyers, with elegant, streamlined designs and top of the line features. However, yacht manufacturers are often tasked with ensuring that a yacht’s components not only look good, but withstand quality performance requirements as well.

A yacht manufacturer recently came to us about upgrading the latching hardware on a transom door that it was installing in a new line of trawler yachts. The manufacturer was not satisfied with the quality of the hardware that came standard with the door, so its engineers were looking for a more dependable, secure latching solution to replace it with.

The manufacturer, however, did not wish to sacrifice the overall aesthetic of the yacht for the sake of functionality, so it specified that any hardware installed must be attractive and complement the yacht’s overall design, as well as all other hardware used throughout.Southco Swim Latch

We suggested Southco’s TM Swim Door Latches, which provide heavy-duty, marine-grade construction suitable for a variety of door thicknesses. The Swim Door Latch features an intuitive operation with push button and turn handle actuation as well as an internal o-ring design that dampens the closing action, providing a smooth end user feel.

Stylish and easy to operate, the Swim Door Latch provides flexibility and functionality for many marine applications, including transom and fly bridge doors, as well as other types of swing doors. Available in 316 stainless steel, these durable latches are resistant to salt spray and the elements.

What challenges have you faced in balancing quality and aesthetics in your yacht design?  Tell us in the comments.

“Hooked” on Interior Railway Design Upgrades

Tuesday, February 14, 2012 by Daniel McCourt
“If the cost of gas goes any higher, I’m taking the train.” Sound familiar? It’s no secret that the ever-rising cost of gas is forcing many commuters to abandon their normal car ride to work and opt for public transportation instead.  In answer, many railway Taking the traincompanies are taking increased ridership by the horns, and making design upgrades to their heavily used railcars.

We recently had a conversation with an engineer who was tasked with redesigning the interior of a local transit company’s  existing railcar. The transit company had requested the engineer to incorporate suggestions obtained through a commuter survey into the design, including improvements to hinges, locking mechanisms embedded in seating.  Of the commuters who provided feedback, a significant number were concerned about having a place to hang their coats, bags and personal belongings during overcrowded peak hours.

Specifically, the engineer was seeking a safe way in which to incorporate coat hooks. In the traditional rail car design, a multi-pronged coat hook protruded from the center of the outer seat panel into the walkway, and often into people forced to stand during peak commuting hours. The challenge was replacing this outdated and potentially dangerous design with something that was both safe and functional.
Southco Coat hook
Our experts suggested Southco’s MP Coat Hook, which remains flush when not in use, and deploys an inner latch, releasing pop-out hook with just the push of a button. It’s ability to remain flush when unused frees up more space, allowing for multiple installations should the design require it. The MP is available with several flange shapes with multiple chrome- or brass-plated finishes to match the stylish new interiors of many mass transportation vehicles – including not only railcars, but buses and airplanes as well.

How will the growth of commuting impact mass transit interior design? Or have an application for a compression latch or position contol hinge you would like to discuss?  Tell us in the comments.

Multi-Point Latching Goes to Great Lengths for Enclosure Cabinet Security

Thursday, February 2, 2012 by Daniel McCourt
Datacenter DesignData center engineers dedicate sizeable amounts of time to designing enclosures, which includes specifying cabinet storage that will ultimately house the complete system.  Factors such as size, materials, rack dimensions, security,  heating and cooling options and the costs associated are all considered by engineers throughout the design, but when it comes to accessibility, it sometimes isn’t approached until the very end of the design process.

We recently had an engineering firm come to us late in the design process with a need to incorporate a multi-point locking system into a tall, upright enclosure door design. The cabinet required a latch that would securely lock its entire length with only one turn. The firm also requested that the system take up minimal space in the overall cabinet design.

Southco engineers suggested one, three-point H3 Swinghandle Multi-point System to secureH3 Swinghandle the enclosure door. When installed, the Swinghandle, which nests into its housing with minimal protrusion, sits on the outside of the cabinet door, and pops up to swing smoothly for easy latch actuation. The cam mechanism sits on the inside of the enclosure door, and a series of rods that run up the entire length of the door are activated by a linear actuator, releasing the latch when the Swinghandle is rotated.

Southco’s H3 is available with multiple offset cams, multi-point latching, and numerous locking and non-locking options that simplify cost-effective configuration. Available in lightweight, robust nylon or heavy-duty die-cast, the H3 is suitable for indoor enclosure cabinet applications across industries.

What types of challenges have you experienced in your enclosure design? Or do you have an application question about latches, hinges or captive fasteners? Tell us in the comments.


Reliable latch technology in a lightweight package

Friday, November 18, 2011 by Daniel McCourt
Electronic rotary action latch light dutyIt seems like everyone is dieting these days…even our products. The new R4-EM Light Duty Electronic Rotary Latch brings the same proven reliability of the standard steel version but has lost a bit of weight—65% to be exact, thanks to its engineered composite plastic construction. But don’t be misled by the compact package; this latch is big in performance.

A microprocessor control brings energy efficiency, and an integrated mechanical override is included for use should a power failure occur.

Need to know the latch status? The optional microswitch will let you know when the door is locked or unlocked. And if you want to monitor and control complete systems remotely, it’s all possible with this latch. Southco Indutry Solutions

The R4-EM is simple to use, simple to install and is concealed for hidden access. Add a 12-24 volt DC power supply (and any access control device), and you have a complete electronic access solution.

Visit our website for more information on the entire line of Rotary Latches or any of our other latches, hinges or electronic access solutions.
 
What do you think of the new R4-EM? Drop us a line.

Two new actuators, one great list of benefits

Friday, October 21, 2011 by Daniel McCourt
On siteIf you’ve ever taken a good look at off-highway equipment that has been left outdoors and exposed to the elements, then you know the damage that is visible from rain, heat and cold.  Well, Southco’s new line of actuators are here, and they are as tough as the elements and are designed for entry door applications. The AC-30 and AC-40 are constructed of corrosion resistant materials and can be used in a wide range of outdoor temperatures.

Both actuators work with Southco R4 rotary latches directlSouthco Actuatory or can be used with cables and rods for a complete rotary latch system. Your equipment will be secure on the job site or roadside due to the key-locking feature with multiple key codes.

The AC-30’s single hole installation enables effective mounting in restricted spaces, and the AC-40 features a large grip handle and single-motion open feature. With the addition of these new actuators, Southco has an even great line of solutions for your most challenging applications. Tell us about it. Or leave a comment. We love to hear from you.

Considering the opening angle: Detent and torque hinges

Monday, August 15, 2011 by Daniel McCourt

Part 4 in a 10-part series on specifying hinges

Door StayWe have all been there: Trying to keep a door open with our foot, a shoe or something else we find lying around. Today’s applications increasingly require hands–free access (or a really patient friend who will hold the door for you). If this is the case with your application, consider using a hinge with a built-in detent feature to hold the door  or panel open at a preset angle. Or use an adjustable-torque feature, which will let you tighten or free up the door swing. Both of these hinge styles eliminate mechanical supports like gas struts or door stays.

Detent and torque hinges are two products in one—the hinge and the doorDetent Hinge stay. They bring with them some nice benefits, too. They reduce the number of parts, cut down on installation time and lower the overall cost.

Most detent hinges come with preset opening angles; some even provide negative angles that let the hinge go slightly past center when closed. This also holds the door securely against the frame and Torque Hingereduces vibration (a viable option when you know you might have rattling!). In some cases, you won’t even need a latch. Detent hinges are most appropriate for small lightweight applications. If this sounds like your application and you can benefit from some of these features, give it a try!
 

Next week: Using removable hinges to access an interior

Design News Article on Designing for Recyclability

Wednesday, July 13, 2011 by Daniel McCourt
Design News LogoDoug Smock over at Design News wrote a great article on Designing for Reyclability this month.  He highlighted the trend towards designing for dissasembly and the key role that fasteners, hinges and latches can play in this effort.

We here at Southco couldn't agree more! Head on over and check it out.

A simple push toward greater convenience

Tuesday, May 24, 2011 by Daniel McCourt
If you’ve ever accidentally closed a door or panel with a traditional cam latch in the closed position, then you know the damage that can occur over time to the door, frame or latch. I have been guilty of this many times myself…

Push to close latchNow, Southco has expanded its E5 Cam Latch selection by adding intuitive push-to close convenience to more than a dozen hand-, tool- and key-actuated models. The push-to-close design prevents damage to the latch regardless of the cam position during closing. A spring-loaded feature automatically engages the cam once it passes the edge of the keeper or frame.

What’s even better is that the new designs satisfy both single-pointE5 Bus and two-point latching options. We all like convenience, and our cam latch installations should be no different! A latched/unlatched status indicator provides users with quick visual confirmation of latch status, too, so there is no more guesswork about whether your panel or door is secured.

E5 EquipmentWhether your application is office furniture, an RV or an electronic enclosure, the E5 has a design and configuration to fit your needs. Simplicity, versatility and flexibility.

To discuss how the flexibility of the new cam latch can enhance your application, send us an email or post a comment.

IFSEC 2011

Monday, May 16, 2011 by Daniel McCourt
Join Southco at the IFSEC 2011 Tradeshow this week.  We will be displaying our latest Electronic Access Solutions at the Isonas booth, Hall 4 4/E160d.

IFSEC 2011Our Applications Engineers will be on hand to answer your toughest implementation challenges.

We look forward to seeing you there!

If you are unable to attend, feel free to email our customer service, available around the world 24/7. They are available to discuss electronic access solutions or any of Southco's 40,000 latches, hinges, or locks.

About IFSEC:

IFSEC is the largest annual security event in the UK.

This year's show saw IFSEC continue to offer unrivalled security solutions to more than 22,743 security professionals.

Dedicated to offering all things security, IFSEC offers you the full spectrum of security products and services available both in the UK and worldwide. Housing 600+ leading manufacturers, suppliers and distributors, the 2010 event had a global reach of over 22,743 attendees from 130 countries and was supported by all industry associations and countless media.


Southco's New Membrane Keypad

Wednesday, May 11, 2011 by Daniel McCourt
Membrane KeypadIt's always nice when a respected publication like PD&D puts one of our new products on their website.

The latest new product to be placed on their site is our EA-KC2 Membrane Keypad Access Controller.

This new keypad can adhere to a frame or door, inside or out. The ability to adhere or be molded into a wide variety of surfaces, combined with connecting it to any one of our Electronic Latches or Locks  brings electronic access to applications that would not have been possible just a few years ago.

Please leave a comment or email us if you would like to hear about some examples of how this new technology is being used in the marketplace.

The EML Goes High(er) Tech

Thursday, April 7, 2011 by Daniel McCourt
There is no question-- electronic record keeping is now the norm. But as the technology has advanced, so too has the opportunity to exploit it. Fortunately, a unique partnership has Biometric Electronic Latchresulted in the industry’s first biometric-integrated latch for computer server racks. Southco has teamed with Digitus Biometrics to secure data right down to the rack level in datacenters.

The db ServerRack access control system marries Southco’s proven H3-EM Electronic Locking Swinghandle with a built-in, multi-stage fingerprint verification and access control system from Digitus Biometrics. It sounds very “CSI,” but it’s actually quite simple and very effective.

The access control unit connects directly to a datacenter’s network via an fingerprintordinary connector. User access to cabinets is then managed from a single desktop. No more keys, cards or PIN pads. And 100% accurate validation! Interfaced with a monitoring network, the system can remotely account for all rack activity, including who accessed it, when it was accessed and the duration. An audit trail has never been simpler. The new db ServerRack access control system includes all needed software and is easily and conveniently retrofitted into existing enclosures. 

To view Southco's entire line of Electronic Latches visit our new dedicated Electronic Access Solutions Mini-site and download a copy of our electronic latching guide.

Stainless Steel Rotary Latch Designed to Meet Challenges of Marine Industry

Tuesday, March 1, 2011 by Daniel McCourt
The ocean can be as unforgiving as it is beautiful when it comes to the harsh effects the sea can have on hinges, latches and other boat hardware.
Stainless Steel Rotary Action Latch
Southco understands the need for a reliable rotary latch that can withstand salt, sun and the damaging effects of water. Hence, the Stainless Steel R4-10 was introduced. The new R4-10 features the same benefits of its zinc-plated predecessor with a finish that delivers durability and corrosion resistance. Constructed of 304 grade stainless steel, the latch can be used in demanding vandal-proof or watertight storage areas with the assurance that its construction meets marine requirements for performance and salt spray resistance. So no more rusted hardware!
 
The R4-10 even offers double stage latching for added security and functionality, so you can rest easy knowing that your belongings are secured against vandals. And a concealed latching option allows flexible styling while the latch accommodates misalignment for a flush, consistent look. The new AC-M1 actuator makes a nice addition, too. It is constructed of 316 grade stainless steel and delivers corrosion resistance and enhanced security.

We want to hear from you! Contact us with your questions or comments on the stainless steel R4-10. Or to learn more about Southco’s line of rotary latches, email us or visit our site at http://www.southco.com

The Mini E-Keeper: A little package with some big benefits

Tuesday, February 1, 2011 by Daniel McCourt


It’s 2/3 the size of its big brother, features an integrated mechanical override and boasts a more efficient gear motor. Meet the Miniature E-Keeper System—a slimmed-down access solution that provides push-to-close operation in one unit.

Southco Miniature Electronic StrikeThis compact unit means that transitioning from mechanical solutions to electronic access solutions could not be simpler. It’s easy to install and can be added right to a frame for use with existing latches. If security is a major concern, it can mounted in a concealed location with remote mechanical override. Which means—yes—it is perfect for applications like medical storage units, postal terminals and other secured enclosures. Put simply, it is designed to simplify access while providing convenience, security and control.
vending machine
Another great thing about the Mini? It’s flexible. So it’ll work with keypads, key fobs, card swipes…an array of different actuation devices. That versatility means you can integrate the specific level of secure access control you require. It accommodates multiple mounting configurations, too, so it can be easily integrated into existing designs. Ahh…secure electronic or manual operation without having to modify enclosure designs. That’ll make OEMs happy!

To share your thoughts on the E-Keeper or learn more about Southco’s complete system offerings, leave us a comment here. We’d love to hear from you!

Safety and Security in The Healthcare Industry

Tuesday, October 19, 2010 by Daniel McCourt
Part 1 of a 2-part series on healthcare access hardware solutions

We all know that safety and security are paramount concerns for the healthcare industry. Providers need to restrict access to patient records, medications and equipment. They need to ensure regulatory compliance. And they often need the ability to monitor systems remotely. It’s a challenge. And it’s one that Southco takes seriously.

Southco has designed its access systems (mechanical and electronic alike) to meet the healthcare industry’s strict measures for increased security and patient safety. 

You can imagine the danger a hospital might face if its secure areas were easily compromised. Whether it’s quarter-turn locks or advanced compression and push-to-close latches, Southco’s mechanical access solutions ensure that information, medication and supplies stay protected. Locks are robust and vandal-resistant, and flexible Key Choice systems offer different locking options. Automatic locking, multipoint systems and stainless steel construction are all features of various mechanical solutions.

But there are instances when managing physical keys is simply not practical or when dealing with  HIPAA requirements. Electronic access solutions such as keypads, electronic keys and RF-based proximity card readers eliminate mechanical keys and work with existing networks. Providers can use these components for remote monitoring, electronic signature and audit trails. What’s also nice is that electronic locks offer programmability that enables automatic relocking, time delays and other unique requirements.

To share your thoughts on healthcare industry challenges or learn more about Southco’s complete system offerings, email us or request your copy of Southco’s Healthcare Access Hardware Guide.
 
Coming Next: Part 2— Ergonomic solutions for the healthcare industry

Data Center World Conference Wrap Up

Tuesday, October 5, 2010 by Daniel McCourt
Data Center World, presented by Afcom hosted their 30 year anniversary tradeshow conference this past weekend in Las Vegas, Nevada on October the 5th. Data Center World is widely considered as the premier tradeshow for central data managers and industry leaders. The conference focuses on data center management and alternatives to securing data within servers through physical and cyber means.

Data center managers have always protected their data through means of either physical and cyber access to server rooms and entry points. Our business development manager, Steve Spatig, spoke at the conference and discussed the importance of physical server security with the application of our electronic access systems. His discussion touched upon different methods of data access security while giving an overview of what is already available in the electronic access market.


Look for a blog from my colleague Maureen Donovan and what she saw at the show in the next few days. I am certain that it will be an entertaining post.  

You can learn more about Southco's Electronic Access Solutions and all of our other latch and hinge solutions at our website, www.southco.com.


Compression Latch Solutions at Innotrans

Monday, September 20, 2010 by Daniel McCourt
This week Southco will be exhibiting at the Innotrans Convention held in Berlin Germany from 21 - 24 September. Innotrans is an International Trade Fair for Transport Technology and has become established as an international industry showplace focusing on Railway Technology.

We'll can be found in Hall 3.1 Stand 220. Stop by and see what over 60 years of constant innovation in compression latch technology can do for you.  Our technical staff will be on hand to answer questions and help solve the most difficult application challenges you show them.

On display will be our stainless steel compression latches, electronic access solutions, and position control technology.

We look forward to seeing you this week!


The Content Marketing Platform Powered by Compendium  |  Sitemap