“Hooked” on Interior Railway Design Upgrades

Tuesday, February 14, 2012 by Daniel McCourt
“If the cost of gas goes any higher, I’m taking the train.” Sound familiar? It’s no secret that the ever-rising cost of gas is forcing many commuters to abandon their normal car ride to work and opt for public transportation instead.  In answer, many railway Taking the traincompanies are taking increased ridership by the horns, and making design upgrades to their heavily used railcars.

We recently had a conversation with an engineer who was tasked with redesigning the interior of a local transit company’s  existing railcar. The transit company had requested the engineer to incorporate suggestions obtained through a commuter survey into the design, including improvements to hinges, locking mechanisms embedded in seating.  Of the commuters who provided feedback, a significant number were concerned about having a place to hang their coats, bags and personal belongings during overcrowded peak hours.

Specifically, the engineer was seeking a safe way in which to incorporate coat hooks. In the traditional rail car design, a multi-pronged coat hook protruded from the center of the outer seat panel into the walkway, and often into people forced to stand during peak commuting hours. The challenge was replacing this outdated and potentially dangerous design with something that was both safe and functional.
Southco Coat hook
Our experts suggested Southco’s MP Coat Hook, which remains flush when not in use, and deploys an inner latch, releasing pop-out hook with just the push of a button. It’s ability to remain flush when unused frees up more space, allowing for multiple installations should the design require it. The MP is available with several flange shapes with multiple chrome- or brass-plated finishes to match the stylish new interiors of many mass transportation vehicles – including not only railcars, but buses and airplanes as well.

How will the growth of commuting impact mass transit interior design? Or have an application for a compression latch or position contol hinge you would like to discuss?  Tell us in the comments.

Safety and Security in The Healthcare Industry

Tuesday, October 19, 2010 by Daniel McCourt
Part 1 of a 2-part series on healthcare access hardware solutions

We all know that safety and security are paramount concerns for the healthcare industry. Providers need to restrict access to patient records, medications and equipment. They need to ensure regulatory compliance. And they often need the ability to monitor systems remotely. It’s a challenge. And it’s one that Southco takes seriously.

Southco has designed its access systems (mechanical and electronic alike) to meet the healthcare industry’s strict measures for increased security and patient safety. 

You can imagine the danger a hospital might face if its secure areas were easily compromised. Whether it’s quarter-turn locks or advanced compression and push-to-close latches, Southco’s mechanical access solutions ensure that information, medication and supplies stay protected. Locks are robust and vandal-resistant, and flexible Key Choice systems offer different locking options. Automatic locking, multipoint systems and stainless steel construction are all features of various mechanical solutions.

But there are instances when managing physical keys is simply not practical or when dealing with  HIPAA requirements. Electronic access solutions such as keypads, electronic keys and RF-based proximity card readers eliminate mechanical keys and work with existing networks. Providers can use these components for remote monitoring, electronic signature and audit trails. What’s also nice is that electronic locks offer programmability that enables automatic relocking, time delays and other unique requirements.

To share your thoughts on healthcare industry challenges or learn more about Southco’s complete system offerings, email us or request your copy of Southco’s Healthcare Access Hardware Guide.
 
Coming Next: Part 2— Ergonomic solutions for the healthcare industry

Compression Latch Solutions at Innotrans

Monday, September 20, 2010 by Daniel McCourt
This week Southco will be exhibiting at the Innotrans Convention held in Berlin Germany from 21 - 24 September. Innotrans is an International Trade Fair for Transport Technology and has become established as an international industry showplace focusing on Railway Technology.

We'll can be found in Hall 3.1 Stand 220. Stop by and see what over 60 years of constant innovation in compression latch technology can do for you.  Our technical staff will be on hand to answer questions and help solve the most difficult application challenges you show them.

On display will be our stainless steel compression latches, electronic access solutions, and position control technology.

We look forward to seeing you this week!

2010 WindPower Conference & Exhibition Blog

Thursday, July 15, 2010 by Maureen Donovan

Wind Energy… Firmly entrenched in Europe wind energy is an exciting opportunity for North America and beyond.  And boy, did the 2010 Wind Power Show in Dallas indicate that.  Over 20,000 attendees and nearly 1400 exhibitors representing companies from countries all over the world including Germany, Spain, Italy, India, Canada, China, Korea and many others.  And the diversity of the offerings was immense… from the largest wind turbines you have ever seen, to the ladders and hoists that allow access and service, to the components inside the turbine that control pitch, power conversion, etc, to the trucking and transport companies responsible for transporting these large turbines and blades across the country.

The excitement at the show was evident, the buzz non-stop.  People are really excited about wind energy taking off in North America.  According to the AWEA, last year the United States installed more than 10,000MW of new wind power.  Thirty six states now have wind projects.  The people were a friendly bunch… happy to discuss opportunities knowing that  we all must all work together to grow this market, both for our companies and the environment.

So let’s talk about the exhibitors.  The turbines are unbelievably large.  Anyone who has ever seen a wind turbine across a field has little idea of the magnitude of these structures.  Or of a single blade.  Or of  the nacelle.  These structures make people look like ants!  All of the major manufacturers were there and it was impressive group.

One of the discussions we had with several of the global exhibitors is the necessity to have local manufacturing around the globe.  It is not economically feasible to ship these large parts all over the world.  Rather the large turbine and blade manufacturers must set up shop regionally, and thus need local suppliers in each region.

Of particular interest to Southco, were the many exhibitors who manufactured equipment for the inside of the turbine.  Many latches, hinges and fasteners could be found on the pitch drives, the inverters and other enclosures in the turbine.   There are a lot pieces of equipment  that need to be accessed during service, and our quarter turn fasteners and compression latches fit the bill..  There are also a lot of applications on the testing equipment, whether it is for monitoring the amount of wind at a location or testing the systems  in the wind turbine.

Other than that there was a lot of just plain fun.  A delicious exhibitor-sponsored lunch was provided each day and offered a good opportunity for networking.  There were plenty of evening activities including a function at the Hard Rock Café featuring Elvis Costello and the Conference Dinner starring Sienfeld’s Jason Alexander.  Even some of the booths got into the spirit of things… The Wind Energy TechnoCentre of Quebec  hired a three-piece Texas jazz band to perform at the end of the day, which led to quite a lively happy hour!

Bottom line is that it is an exciting time for green energy worldwide and especially wind. 
The growth potential is enormous and the clean energy it can provide is ELECTRIFYING!

Chassis Components for a Rugged Environment

Thursday, June 10, 2010 by Daniel McCourt
Part 2 of a 3-part series on off-highway access components

Large EquipmentFlying stones and sand. Extreme temperatures. Harsh vibration and corrosion. Most off-highway vehicles endure an endless assault from their environment. Southco understands the unique stresses of the off-highway industry and has crafted its chassis access hardware to be robust and reliable.

If you work in the off-highway or construction industries, then it won’t be hard to imagine a piece of equipment hauling several tons of excavated material over the uneven terrain of a construction site. A lot of energy can be translated through the vehicle while on site. Keeping access panels and doors closed requires hardware that is designed for these situations. Southco's folding t-handle compression latches have been engineered to withstand high loads, shock and vibration. These types of latches feature a rugged “lift and turn” operation that promises both dependability and a comfortable grasp.

To avoid having to worry about a stone or a piece of debris disabling your ability to open a door or access panel, a concealed rotary latch is an ideal solution. Paired with a cable system and a remote actuator, these latches offer the convenience of push button actuation and the confidence of positive latch engagement.

Southco’s chassis solutions are designed to ensure rugged durability in harsh conditions. When you latch a hood, it will stay latched. (No more rattling!) And you will enjoy convenient access for engine covers, storage compartments and access panels.

To share your thoughts on entry door solutions or learn more about Southco’s complete system offerings, email us or download your copy of our Design Guide today.
 
Coming Next: Part 3— Off-highway Interiors: Safety, Comfort and Convenience

CTT Conference, Moscow Russia

Tuesday, May 25, 2010 by Daniel McCourt


Next week we'll be exhibiting at the CTT Conference in Moscow, Russia. If you are attending the show, please join us at Booth 3-341 in Hall 3.  The team is looking forward to speaking with our customers and learning more about their needs.

We'll be displaying our latest innovative products for the off-highway and construction industries.  Stop by and be the first to see these new products:


      Heavy Duty Lift and Turn Compression Latches





      Single Point Actuators






RF Wireless Remote Controller







Electronic Rotary Latches





The delicate balance in achieving the “wow” factor

Tuesday, August 4, 2009 by Daniel McCourt
You only have to glance at newspaper headlines or Wall Street numbers to understand the current state of the economy. More than ever, CFOs everywhere are keeping a close eye on the bottom line in these lean times. Design engineers also face the daily challenge of simplifying production and minimizing unit costs. It’s no easy task.


While considering cost, design engineers are also devising more complex and sophisticated designs that are ergonomic, functional, stylish and as my son would say, "cool". Every designer strives for that “wow” reaction when a customer eyes his or her product. Competition is getting stronger in almost every market.

Designers are constantly challenged with the delicate balance among performance, style and cost.

 
At Southco, we’ve learned how Touchpoint Engineering can help designers achieve greater product differentiation, more trouble-free performance and more cost-effective production. Increasingly, it’s the little things that provide the visceral reaction from consumers—the smooth and balanced feel of a torque hinge in a LCD screen on a piece of medical equipment,  the look of a polished chrome compression latch, or perhaps the innovation of an electronic latch — so why not harness the potential value of Touchpoint Engineering in making these elements product differentiators?


By addressing the full scope of access hardware early on, designers can stand out from the pack with products that are superior in look and functionality and that are ...cool.


Feel free to leave a comment or contact us with your design challenges.

The Content Marketing Platform Powered by Compendium  |  Sitemap