Tag: audit trail

New Junction Box Facilitates Electronic Access Integration for Server Cabinets

Southco's new EA-A01 SSI  uses the H3-EM Electronic Swinghandle to integrate directly with the building security system.
Southco’s Security System Integration Kit simplifies connectivity between building access systems and the H3-EM Electronic Swinghandle line.

In response to data protection industry regulations, many data centers are networking server racks to their existing security systems to monitor and control physical access to the racks, just as they do for building and room access.

Southco’s EA-A01 Security System Integration Kit simplifies the cabling and connections necessary between electronic locking solutions, such as Southco’s H3-EM Electronic Swinghandle with Integrated Prox Reader and any Wiegand based access control system.

The Integration Kit features easy plug-and-play installation, integrating with existing building access control infrastructure and extending data center security down to the rack level using readily available structured cabling. This complete turnkey solution offers a simple, cost effective way to leverage existing systems to control and monitor access at the rack level within the data center.

3771087063_17a079c2cc_z
New Racks by Docklandsboy CC-BY-2.0

When integrated with an existing access control system, the new Integration Kit facilitates complete remote control and monitoring from building and room access down to server door access, which demonstrates compliance with regulatory requirements such as HIPAA, HITECH and PCI DSS.

To learn more about our solutions for electronic access and control, visit Southco’s Electronic Access Solutions minisite.

3 Ways Electronic Access Control Can Improve Data Center Security in 2014

With 2014 fast approaching, updating data center security systems for the new year is a key concern. The increased level of enforcement of U.S. data protection regulations in 2014 (HIPAA and PCI DSS, for example) has many IT professionals turning to increased physical security measures to protect confidential data. These measures include remotely monitor

Enhancing Security In New Self Service Kiosk Designs

Designers are constantly developing new uses for enclosures and kiosks that take the concept of Self Service to the next level. With the introduction of high-value retail and vending kiosks and “intelligent vending” systems, Self Service providers have identified a need for more enhanced physical security solutions that can be controlled and monitored re

Improving Kiosk Design with Concealed Electronic Latches

One of the most important aspects of any Self Service kiosk or enclosure design is not only what it does, but how it looks to the consumer. Therefore, design engineers must balance aesthetic appeal with usability in order to execute effective Self Service design. Many modern kiosks feature a 360 degree design – meaning that they are viewable from all an

Replacing Mechanical Locks with Electronic Locks on Medical Enclosures

In today’s healthcare facilities, security threats extend beyond physical building security and down to medical enclosures such as cabinets, dispensing carts and charting stations, and portable diagnostic equipment. For many healthcare facility managers, monitoring security at the enclosure or cart level can be a challenge. In response, many are looking to

Best Practices for Electronic Lock Selection for Self-Service Applications

When designing physical security into self-service enclosures, such as kiosks and pick-up drop-off points (PUDOs), manufacturers must anticipate the need for modern methods of access control and incorporate new technology, while still providing a solution that is cost-effective and meets the requirements of the growing self-service industry. Incorporating ap

Biometric Latching: Security with a Personal Touch

When issuing security cards, codes and keys, it is often difficult to guarantee that only the individuals authorized to use these items will actually do so. Though it may be against company policy, an employee may still allow a co-worker to borrow his/her key for the sake of convenience. Even with the latest technology-based security and audit solutions, tra

New and Improved Electronic Swinghandle Features Built-in Proximity Reader

Southco’s popular electronic swinghandle is now available with an integrated proximity reader, allowing our customers to seamlessly add additional keyless entry points to existing security systems. Southco’s new H3-EM Electronic Locking Swinghandle with Integrated Proximity Reader produces a standard 26 bit Wiegand output and accepts HID 125 kHz pro

Security at the Cabinet Level: Electronic Locking Solutions That Won’t Get Lost in the Cloud

Cloud computing is not just a technology buzz phrase anymore – it’s a reality. As more companies begin moving their data (and customer data) to the cloud, the focus is not just on the new technology itself, but on securing datacenters and protecting information from the threat of security breaches. While many precautions can be taken software-wise whe

Electronic Latching Protects Access to Pharmaceuticals

In hospitals, pharmaceutical theft is a big problem. Medicine that is unaccounted for or dispensed of improperly can cause disruptions to patient care, and in severe cases, these actions can even result in accidental death. To prevent pharmaceutical theft from occurring, the medical industry must implement access solutions that not only keep pharmaceutical i