Tag: datacenter

Case Study: AKCP Improves DCIM Security with Southco Electronic Locks

The data center market is constantly expanding as businesses continue to adopt cloud computing within their organizations. With the demand for cloud computing services rapidly increasing, data centers are implementing highly reliable data center infrastructure management (DCIM) solutions to control physical access to the cabinets that secure valuable data.

AKCess Pro (AKCP), one of the world’s largest manufacturers of networked environmental power, security and access control monitoring equipment, recently partnered with Southco to expand its DCIM solutions to include intelligent electronic locks. Considering company reputation for product quality and market share, AKCP selected Southco’s H3-EM Electronic Locking Swinghandle series to integrate into its existing DCIM solutions.

Southco H3-EM series
Electronic locks, like Southco’s H3-EM Swinghandle series provide an extra layer of security for data center cabinets (shown here integrated with AKCP’s DCIM solutions).

The integration of Southco’s electronic access solutions and AKCP’s DCIM solutions allows the data center service provider to easily manage the security system from a central location. When customers or visitors want access to certain locations or servers within the infrastructure, AKCP’s facility manager can remotely unlock the door rather than physically walking to the area, increasing work efficiency.

The integrated solutions enable real-time monitoring within the premises. When alerted to a potential security threat, staff is immediately notified by the alarm system to ensure the data stored in the servers is secure. AKCP also benefits from the simple reporting system that Southco’s integrated solutions provide. A digital report of access and summary of activities can be quickly generated, saving resources previously dedicated to manual report creation, ultimately streamlining the process.

“Southco’s solution met our rigorous standard tests and performed well in all of our onsite trials with multiple cabinets and with our software. With a large selection of hardware and a commitment to quality that AKCP requires of its partners, and the fact that the server cabinet lock and handle from Southco worked so well, working with Southco gave us more hardware options for server cabinets, allowing us to better serve our clients,” added Nicholas Barrowclough, Vice President of Production at AKCP.

The compatibility of Southco’s products with AKCP’s existing system was a major factor contributing to this partnership. Southco’s electronic locks offer easy, plug-and-play installation, allowing them to fit many of the cabinets that are popular in data centers today. Upon integration of Southco’s EAS into AKCP’s DCIM solutions, the data center service provider can now simplify their operations and save resources by central controlling access to certain locations or servers, allowing real-time monitoring within the premises, and generating a digital report of access to streamline the reporting process.

“We like Southco’s large product line as our clients wants us to integrate a wide variety of locks, sensors and software,” said Charles Meyer, Senior Hardware Engineer at AKCP. “Being able to accommodate requests for traditional style locks and hinges, as well as electronic server cabinet locks with one company makes ordering more convenient. In addition, it provides increased security, as well as helps us to comply with company and regulatory requirements.”

AKCP has continued to expand its market share since the integration of Southco’s EAS into its DCIM solutions. “Our door control unit and cabinet control unit allow our clients to expand their security measures within their budgets,” said David Reid, Vice President of Operations of AKCP. “Southco’s security offering gives us the required level of security a data center service provider needs, and we are able to make better use of our resources to deliver higher-value service to our customers.”

To learn more about Southco’s electronic locks and access control options, visit our Data Center micro site.

New Junction Box Facilitates Electronic Access Integration for Server Cabinets

In response to data protection industry regulations, many data centers are networking server racks to their existing security systems to monitor and control physical access to the racks, just as they do for building and room access. Southco’s EA-A01 Security System Integration Kit simplifies the cabling and connections necessary between electronic l

Southco Engineering Article Roundup

Did you know that Southco’s thought leaders are often featured in industry publications and online resources around the web? In case you missed it, we would like to share a few recent articles that showcase our diverse engineering and technology expertise and provide value to the markets we serve. Check out the following stories in our Engineering A

3 Ways Electronic Access Control Can Improve Data Center Security in 2014

With 2014 fast approaching, updating data center security systems for the new year is a key concern. The increased level of enforcement of U.S. data protection regulations in 2014 (HIPAA and PCI DSS, for example) has many IT professionals turning to increased physical security measures to protect confidential data. These measures include remotely monitor

Multi-Point Flat Rod Latching: An Enclosure’s Best Defense

Southco’s new A5 Multi-Point Flat Rod System is an economical, complete solution that offers increased strength when controlling multiple latching points from a single point of operation. The flat design provides an economical solution with added strength in enclosure applications with longer doors and panels, eliminating flexing, pry points and rattle.

Join Southco at AFCOM DCW and IBEX In October!

Southco is hitting the road in October to exhibit our access hardware solutions at two upcoming conferences: AFCOM Data Center World and the International Boatbuilders' Exhibition. Beginning Sept. 30 and through Oct. 3, Southco will exhibit in Booth 631 at Fall Data Center World Conference in Nashville, Tennessee. Stop by to see our newly launched H3

New and Improved Electronic Swinghandle Features Built-in Proximity Reader

Southco’s popular electronic swinghandle is now available with an integrated proximity reader, allowing our customers to seamlessly add additional keyless entry points to existing security systems. Southco’s new H3-EM Electronic Locking Swinghandle with Integrated Proximity Reader produces a standard 26 bit Wiegand output and accepts HID 125 kHz pro

Now You Can Control 14 Different Electronic Locks and Devices From One Computer

Southco’s newest technology allows you to seamlessly actuate multiple electronic locks and devices through your existing computer. Southco’s EA-A06 USB Controller provides simple, independent, remote actuation of up to 14 electromechanical latches when connected to a standard computer USB port. The EA-A06 is designed with plug-and-play functionality w

Security at the Cabinet Level: Electronic Locking Solutions That Won’t Get Lost in the Cloud

Cloud computing is not just a technology buzz phrase anymore – it’s a reality. As more companies begin moving their data (and customer data) to the cloud, the focus is not just on the new technology itself, but on securing datacenters and protecting information from the threat of security breaches. While many precautions can be taken software-wise whe

Compact Prox Card Reader Offers Simplified, Keyless Access

Southco’s EA-P3 Proximity Reader provides convenient, secure access control of electronic locking devices in a compact package. The EA-P3 produces a standard 26 bit Wiegand output and accepts HID 125 kHz prox cards or tags, allowing it to be easily combined with an existing access controller to add additional keyless entry points to existing security syste