Enclosures

Southco's access hardware is designed to make your enclosures secure, attractive, and function smoothly.

Removable hinges and interior access


Part 5 in a 10-part series on specifying hinges

ServicemanSometimes a user or service technician requires full access to the interior of a cabinet or enclosure. If this is the case,  lift-off hinges or hinges with retractable pins can make it quick and easy to remove a door. You’ll also find these hinges valuable if a product ships unassembled or if the door and frame are manufactured in different locations.

Lift-off hinges let you remove the door in a single motion (withoutLift Off Hinge using tools). Just lift the door off the hinge pins mounted to the frame, and replace it by lowering it back over the hinge pins. Both your hands will remain free to maneuver the door. It might be a two-person job at most, but you’ll be amazed at the ease and speed of removal these hinges allow.

Hinges with retractable pins enable door removal without ever having to lift it. You retract the hinge pins and pull the door straight off. To replace it, you would just need to align the two halves of the hinge, Pin Lift Off Hingeextend the pins and lock the door back into place. Quick and very simple. While hinges with pins permanently attached won’t let the hinges drop or get lost, retractable hinge pings might be a better choice if the hinge axis is not guaranteed to remain vertical and steady.

Next week: Working within industry specifications

Deciding between concealed and externally mounted hinges

Part 3 in a 10-part series on specifying hinges We’ve discussed how important a consideration strength is when selecting a hinge. Now it’s time to examine the design considerations that sometimes dictate whether we select a concealed or externally mounted hinge. Concealed hinges mount on the interior part of the door and frame. They are great to us

How strong of a hinge do you really need?

Part 2 in a 10-part series on specifying hinges Last week we discussed how strength is often one of the first considerations when choosing a hinge. But just how strong a hinge do you need? Here at Southco we use four factors that can help when getting started. 1. Weight: Determine the weight of the door. If you can’t physically weigh the door on a

Incorporate hinges early to save money and frustration

Part 1 in a 10-part series on specifying hinges It is not uncommon to wait until the last minute to incorporate hinges into a design.  We know that not everyone has hinges at the top of their list of important things to think of when working on a new car, enclosure, or life-saving medical device.. However, considering hinges late in the design cycle can

CMEF Exhibition 2009

Well almost directly from Chicago, it was off to Shenzhen China for the China International Medical Equipment Fair (CMEF). Once again we were featuring our Position Control Technology, displaying our new line of friction hinges, and our soon to be released monitor arm. We were visited by internationally known medical device manufacturers such as Mindray, Lan